Read-only
About FIFO

DataCount Property


Description

Returns the total number of data points in the FIFO buffer.

 VB Syntax

value = fifo.DataCount

Variable

(Type) - Description

value

(Long Integer) Variable to store the returned number of data points.

fifo

A FIFO Object

Return Type

Long Integer

Default

Not Applicable

Examples

value = fifo.DataCount 'Read

C++ Syntax

HRESULT get_DataCount(long *value)

Interface

IFIFO