| Write/Read | About SA Application | 
| Description | Enables/disables data level threshold mode. Set the threshold level using the DataLevelThreshold command. | 
| VB Syntax | sa.dft.DataLevelThresholdEnabled = value | 
| Variable | (Type) - Description | 
| sa.dft | A SpectrumAnalyzerDFT (object) | 
| value | (Boolean) Choose from: 0 - OFF - Disable threshold mode. 1 - ON - Enable threshold mode. | 
| Return Type | Boolean | 
| Default | OFF | 
| Examples | sa.dft.DataLevelThresholdEnabled = ON 'Write | 
| value = sa.dft.DataLevelThresholdEnabled 'Read | |
| C++ Syntax | HRESULT get_DataLevelThresholdEnabled(VARIANT_BOOL* 
		 enable) | 
| Interface | ISpectrumAnalyzerDFT2 |