| Write / Read | About Cal Sets | 
| Description | Sets or returns the descriptive string assigned to the Cal Set. Change this string so that you can easily identify each Cal Set constructed. | 
| VB Syntax | CalSet.Description = value | 
| Variable | (Type) - Description | 
| CalSet | (object) - A Cal Set object | 
| value | (string) – Description of the Cal Set | 
| Return Type | String | 
| Default | “CalSet_n” where n is an integer number. | 
| Examples | CalSet.Description = "My Cal Set" 'Write | 
| C++ Syntax | HRESULT get_Description(BSTR *pVal) HRESULT put_Description(BSTR newVal); | 
| Interface | ICalSet |