Write/Read |
About Path Configurator |
Description |
Write and read descriptive text associated with the configuration. This text is displayed in the path configuration dialog. Text is generally used to describe external connections that must be made manually to complete the configuration setup. |
VB Syntax |
pathConfig.DescriptiveText = text |
Variable |
(Type) - Description |
name |
(String) Variable to store the returned configuration name. |
pathConfig |
A PathConfiguration (object) |
text |
(String) Descriptive text enclosed in quotes. |
Return Type |
String |
Default |
Not Applicable |
Examples |
pathConf.DescriptiveText "here are the instructions for connecting the device for this configuration" |
C++ Syntax |
HRESULT get_DescriptionText(BSTR* pConnectionText ); HRESULT put_DescriptionText(BSTR connectionText ); |
Interface |
IPathConfiguration |