Read-Only
About External Devices

DeviceNames Property


Description

Returns a list of configured device names of the specified device type.

 VB Syntax

value = extDevices.DeviceNames(devType)

Variable

(Type) - Description

value

(Variant) Variable to store the device names.

extDevices

An ExternalDevices (collection)

devType

(String) Device Type such as "Source" and "Power Meter". See a complete list of valid device types.

Return Type

Variant Array

Default

Not Applicable

Examples

devices = extDevices.DeviceNames("Power Meter" ) 'Read

C++ Syntax

HRESULT get_DeviceNames(VARIANT *names);

Interface

IExternalDevices2