Write/Read |
|
Description |
Set and read the repeat count for the specified dimension order in the multi-dimensional sweep. |
VB Syntax |
md.DimensionRepeatCount (dim) = value |
Variable |
(Type) - Description |
md |
A MultiDimensionalSweep (object) which belongs to a SA channel. |
dim |
(long) Dimension order. Choose an integer value of 1 or higher. |
value |
(long) Repeat count. Choose an integer value of 1 or higher. |
Return Type |
long |
Default |
1 |
Examples |
md.DimensionRepeatCount (2) = 1 'Write |
value = md.DimensionRepeatCount(4) 'Read |
|
C++ Syntax |
HRESULT put_ DimensionRepeatCount (long dim, long value); HRESULT get_ DimensionRepeatCount (long dim, long* value); |
Interface |
IMultiDimensionalSweep |