Write/Read
About Distance MarkerSettings

DistanceMarkerMode Property


Description

Specifies the measurement type in order to determine the correct marker distance.

  • Select Auto for S-Parameter measurements.

  • Select Reflection or Transmission for arbitrary ratio or unratioed measurements.

This settings affects the display of ALL markers for only the ACTIVE measurement.

 VB Syntax

trans.DistanceMarkerMode = value

Variable

(Type) - Description

trans

A Transform (object)

value

(enum As NADistanceMarkerMode) - Choose from:

0 - naDistanceMarkerModeAuto

1 - naDistanceMarkerModeReflection

2 - naDistanceMarkerModeTransmission

Return Type

Enum

Default

0 - naDistanceMarkerModeAuto

Examples

trans.DistanceMarkerMode = naDistanceMarkerModeReflection 'Write

DMM = trans.DistanceMarkerMode 'Read

C++ Syntax

HRESULT get_DistanceMarkerMode(tagNADistanceMarkerMode *pVal);

HRESULT put_DistanceMarkerMode(tagNADistanceMarkerMode newVal);

Interface

ITransform2