Write/Read
About Distance MarkerSettings

DistanceMarkerUnit Property


Description

Specifies the unit of measure for the display of marker distance values. This settings affects the display of ALL markers for only the ACTIVE measurement (unless Distance Maker Units are coupled using CoupledParameters Property.

 VB Syntax

trans.DistanceMarkerUnit = value

Variable

(Type) - Description

trans

A Transform (object)

value

(Enum As NADistanceMarkerUnit) - Distance Marker Units. Choose from

0 - naDistanceMarkerUnitMeter

1 - naDistanceMarkerUnitFeet

2 - naDistanceMarkerUnitInch

Return Type

Enum

Default

0 - naDistanceMarkerUnitMeter

Examples

trans.DistanceMarkerUnit = naDistanceMarkerUnitFeet 'sets the

U = trans.DistanceMarkerUnit 'Read

C++ Syntax

HRESULT get_DistanceMarkerUnit(tagNADistanceMarkerUnit *pVal);

HRESULT put_DistanceMarkerUnit(tagNADistanceMarkerUnit newVal);

Interface

ITransform2