DrawLimitLinesInRed Property

Write/Read
About Limit Lines

Description

Set and return whether to draw limits lines in Red or the trace color.

 VB Syntax

pref.DrawLimitLinesInRed = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Boolean) - Choose from:

True - All Limit lines are drawn in Red.

False - Limit lines are drawn the same color as the trace.

Return Type

Boolean

Default

False

Examples

pref.DrawLimitLinesInRed = True 'Write

value = pref.DrawLimitLinesInRed 'Read

C++ Syntax

HRESULT get_DrawLimitLinesInRed (VARIANT_BOOL* preference);

HRESULT put_DrawLimitLinesInRed (VARIANT_BOOL val)

Interface

IPreferences15