Write/Read
About ExternalDevices

DwellPerPoint Property


Description

Sets and returns the amount of time the VNA should wait after for an external source to settle before making a measurement at each data point.

 VB Syntax

extSource.DwellPerPoint = value

Variable

(Type) - Description

chan

An ExternalSource (object)

value

(Double) Dwell time in milliseconds.

Return Type

Double

Default

3

Examples

extSource.DwellPerPoint = 10 'Write

dpp = extSource.DwellPerPoint 'Read

C++ Syntax

HRESULT get_DwellPerPoint (tagNAExtDevDwellPerPoint *pValue)
HRESULT put_DwellPerPoint (tagNAExtDevDwellPerPoint newVal)

Interface

IExternalSource