Read-only

ECALModuleNumberList Property


Description

Returns a list of index numbers to be used for referring to the ECal modules that are currently attached to the VNA.

 VB Syntax

clist = cal.ECALModuleNumberList

Variable

(Type) - Description

clist

Variable to store the returned list of index numbers.

cal

Calibrator (object)

Return Type

Variant

Default

Not Applicable

Examples

clist = cal.ECALModuleNumberList
'If 2 modules are attached to the VNA
'then the returned list will be:

1,2

C++ Syntax

HRESULT get_ECALModuleNumberList( VARIANT *modules);

Interface

ICalibrator6