Write/Read

 

ElecDelayMedium Property


Description

Sets or returns the electrical delay medium.

 VB Syntax

meas.ElecDelayMedium = value

Variable

(Type) - Description

meas

A Measurement  (object)

value

( enum NACalStandardMedium ) choose from

0 - naCoax

1 - naWaveGuide

Return Type

NACalStandardMedium

Default

Not Applicable

Examples

Print meas.ElecDelayMedium 'prints the value of the electrical delay medium

C++ Syntax

HRESULT get_ElecDelayMedium(tagNACalStandardMedium *pVal);

HRESULT put_ElecDelayMedium(tagNACalStandardMedium newVal);

Interface

IMeasurement2