| Write/Read | About SA Application | 
| Description | Set and read enable force ADC record size mode. | 
| VB Syntax | sa.EnableForceADCRecordSize = value | 
| Variable | (Type) - Description | 
| sa | A SpectrumAnalyzer (object) | 
| value | (Boolean) Choose from: 0 - OFF - ADC record size set automatically. 1 - ON - Manually set ADC record to specified size using ForceADCRecordSize. | 
| Return Type | Boolean | 
| Default | 0 | 
| Examples | sa.EnableForceADCRecordSize = AUTO 'Write | 
| value = sa.EnableForceADCRecordSize 'Read | |
| C++ Syntax | HRESULT put_EnableForceADCRecordSize(VARIANT_BOOL bEnable); HRESULT get_EnableForceADCRecordSize(VARIANT_BOOL* bEnable); | 
| Interface | ISpectrumAnalyzer |