Write/Read |
About VNA-Pulse Generators |
Description |
Enables/disables modulator and ADC delays for pulse measurements. |
VB Syntax |
pulse.EnableOffsetDelays = value |
Variable |
(Type) - Description |
pulse |
A PulseGenerator (object) |
value |
(Boolean) Choose from: ON (or 1) - Enable delays. OFF (or 0) - Disable delays. |
Return Type |
Boolean |
Default |
False |
Examples |
pulse.EnableOffsetDelays = True 'Write |
bool = pulse.EnableOffsetDelays 'Read |
|
C++ Syntax |
HRESULT get_EnableOffsetDelays(VARIANT_BOOL* enable); HRESULT put_EnableOffsetDelays(VARIANT_BOOL enable); |
Interface |
IPulseGenerator5 |