Write/Read
About External DC Devices

ErrorQuery Property


Description

Sets and returns the Error Query command for an external DC Source and an external DC Meter.

 VB Syntax

extDC.ErrorQuery = value

Variable

(Type) - Description

extDC

A ExternalDCDevice (object)

value

(String) The SCPI command for returning DC Source and DC Meter errors.

Return Type

String

Default

"SYST:ERR?"

Examples

extDC.ErrorQuery = "SYST:ERR?" 'Write

value = extDC.ErrorQuery 'Read

C++ Syntax

HRESULT get_ErrorQuery( BSTR* cmd);

HRESULT put_ErrorQuery( BSTR cmd);

Interface

IExternalDCDevice3