| Write/Read | About SA Application | 
| Description | Enables/disables exporting data to the FIFO (First-IN, First-OUT) data buffer. FIFO is a circular buffer that allows very fast Read-Write access. Note: FIFO commands are under the FIFO Object, and a new set of commands has been added here for binary data. | 
| VB Syntax | sa.dft.FIFOEnabled = value | 
| Variable | (Type) - Description | 
| sa.dft | A SpectrumAnalyzerDFT (object) | 
| value | (Boolean) Choose from: 0 - OFF - Export data to FIFO disabled. 1 - ON - Export data to FIFO enabled. | 
| Return Type | Boolean | 
| Default | OFF | 
| Examples | sa.dft.FIFOEnabled = ON 'Write | 
| value = sa.dft.FIFOEnabled 'Read | |
| C++ Syntax | HRESULT get_FIFOEnabled(VARIANT_BOOL* enable) | 
| Interface | ISpectrumAnalyzerDFT |