Write/Read
About SA Application

FileEraseEachSweep Property


Description

Enables/disables erasing output data files after each sweep. When disabled, data is appended to the output file after each sweep which could lead to very large files sizes (and eventually fill the disk).

 VB Syntax

sa.dft.FileEraseEachSweep = value

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Boolean) Choose from:

0 - OFF - Erase data files after each sweep disabled.

1 - ON - Erase data files after each sweep enabled.

Return Type

Boolean

Default

ON

Examples

sa.dft.FileEraseEachSweep = ON 'Write

value = sa.dft.FileEraseEachSweep 'Read

C++ Syntax

HRESULT get_FileEraseEachSweep(VARIANT_BOOL* enable)
HRESULT put_FileEraseEachSweep(VARIANT_BOOL enable)

Interface

ISpectrumAnalyzerDFT