Read only
About VNA Options

FirmwareMajorRevision Property


Description

Returns the major firmware revision number as an integer. For example, given a firmware revision number A.03.30, this command returns 3.

 VB Syntax

value = cap.FirmwareMajorRevision

Variable

(Type) - Description

value

(Long) - Variable to store the returned integer value of the firmware revision number.

cap

A Capabilities (object)

Return Type

Long

Default

Not Applicable

Examples

value = cap.FirmwareMajorRevision 'Read

C++ Syntax

HRESULT get_FirmwareMajorRevision(long * majorRev );

Interface

ICapabilities