Read-only
About VNA-Pulse Generators

ADCDelay Property


Description

Returns the ADC delay for pulse measurements.

 VB Syntax

value = pulse.ADCDelay

Variable

(Type) - Description

pulse

A PulseGenerator (object)

value

(Double) - Variable to store the returned ADC delay.

Return Type

Double

Default

Not Applicable

Examples

value = pulse.ADCDelay 'Read

C++ Syntax

HRESULT get_ADCDelay(double* delay);

Interface

IPulseGenerator5