Write/Read
About Noise Figure

ForceDeEmbedENRAdapter Property


Description

Set and read the De-embedENRAdapter state. Learn more.

 VB Syntax

noiseCal.ForceDeEmbedENRAdapter = value

Variable

(Type) - Description

noiseCal

A NoiseCal (object)

value

(boolean) - ENR Adapter de-embed state.

False - Do not Force de-embedding.

True - Force de-embedding.

Return Type

Boolean

Default

False

Examples

noiseCal.ForceDeEmbedENRAdapter = False 'Write

AdapterDembed = noiseCal.ForceDeEmbedENRAdapter 'Read

C++ Syntax

HRESULT get_ForceDeEmbedENRAdapter(VARIANT_BOOL* on);

HRESULT put_ForceDeEmbedENRAdapter(VARIANT_BOOL on);

Interface

INoiseCal2