Write/Read
About Noise Figure

ForceDeEmbedThruAdapter Property


Description

Sets and reads the state of Thru adapter de-embedding. Learn more.

 VB Syntax

noiseCal.ForceDeEmbedThruAdapter = value

Variable

(Type) - Description

noiseCal

A NoiseCal (object)

value

(boolean) - Thru Adapter de-embed state.

False - Do not Force de-embedding.

True - Force de-embedding.

Return Type

Boolean

Default

False

Examples

noiseCal.ForceDeEmbedThruAdapter = False 'Write

AdapterDembed = noiseCal.ForceDeEmbedThruAdapter 'Read

C++ Syntax

HRESULT get_ForceDeEmbedThruAdapter(VARIANT_BOOL* on);

HRESULT put_ForceDeEmbedThruAdapter(VARIANT_BOOL on);

Interface

INoiseCal4