Write/Read |
About Auxiliary Triggering |
Description |
Turns handshake ON / OFF. To enable handshake, the main trigger enable must ALSO be set using Enable. When ON, VNA acquisition waits indefinitely for the input line to be asserted before continuing with the acquisition. Note: Use on PNA-X ONLY. Other models do NOT have an Aux Input. |
VB Syntax |
auxTrig.HandshakeEnable = state |
Variable |
(Type) - Description |
auxTrig |
An AuxTrigger (object) |
state |
(boolean) - True - Handshake enabled False - Handshake NOT enabled |
Return Type |
Boolean |
Default |
False |
Exaamples |
auxTrig.HandshakeEnable = True 'Write |
value = auxTrig.HandshakeEnable 'Read |
|
C++ Syntax |
HRESULT get_HandshakeEnable(VARIANT_BOOL * enable); |
Interface |
IAuxTrigger |