Read only
About VNA Options

HasDirectReceiverAccess Property


Description

Returns whether or not the analyzer has direct receiver access (front-panel jumpers).

 VB Syntax

value = cap.HasDirectReceiverAccess

Variable

(Type) - Description

value

(Boolean) - Variable to store the returned value

True - VNA has direct receiver access.

False - VNA does NOT have direct receiver access.

cap

A Capabilities (object)

Return Type

Boolean

Default

Not Applicable

Examples

value = cap.HasDirectReceiverAccess 'Read

C++ Syntax

HRESULT get_HasDirectReceiverAccess(VARIANT_BOOL *present );

Interface

ICapabilities12