Read-only
About LFE

HasLowFrequencyExtension Property


Description

Returns whether or not the VNA has the low frequency extension (LFE) installed. Learn more.

 VB Syntax

value = chan.HasLowFrequencyExtension

Variable

(Type) - Description

value

(boolean)

False - LFE is not installed.

True  - LFE is installed.

cap

Capabilities (object)

Return Type

Not applicable

 

hasLFE = cap.HasLowFrequencyExtension 'Read

C++ Syntax

HRESULT get_HasLowFrequencyExtension(VARIANT_BOOL* hasLFE);

Interface

ICapabilities16