Write/Read |
About SA Application |
Description |
Set and read the show / hide state of the image reject traces in the measurement parameters dialog. |
VB Syntax |
sa.EnableImageRejectTraces = value |
Variable |
(Type) - Description |
|
sa |
A SpectrumAnalyzer (object) |
|
value |
(Boolean) Choose from: 0 - OFF -Disable image reject traces. 1 - ON - Enable image reject traces and set mode using ImageReject. |
Return Type |
Boolean |
Default |
0 |
Examples |
sa.EnableImageRejectTraces = 0 'Write |
|
value = sa.EnableImageRejectTraces 'Read |
|
C++ Syntax |
HRESULT put_EnableImageRejectTraces(VARIANT_BOOL bEnable); HRESULT get_EnableImageRejectTracesVARIANT_BOOL* bEnable); |
Interface |
ISpectrumAnalyzer |