Write/Read |
About Noise Figure |
Description |
Sets the number of impedance states to use during calibrated measurements. |
VB Syntax |
noise.ImpedanceStates = value |
Variable |
(Type) - Description |
noise |
A NoiseFigure (object) |
value |
(double) - Impedance states. Choose between 4 and the maximum number allowed by the noise tuner device. If the specified number exceeds the capability of the device, the measurement will use the maximum number of states the device allows. |
Return Type |
Double |
Default |
4 |
Examples |
noise.ImpedanceStates = 10 'Write |
AvgNoise = noise.ImpedanceStates 'Read |
|
C++ Syntax |
HRESULT get_ImpedanceStates(double* pVal) HRESULT put_ImpedanceStates(double newVal) |
Interface |
INoiseFigure |