Write/Read |
About Phase Reference Cals |
Description |
Sets and returns the state of Unknown Mixer calibration. |
VB Syntax |
phaseRef.IncludeUnknownMixer = value |
Variable |
(Type) - Description |
object |
PhaseReferenceCalibration (object) |
value |
(Boolean) Unknown Mixer cal state. Choose from: True - Enable Unknown Mixer cal. The start frequency becomes 10 MHz and can NOT be changed. False - Disable Unknown Mixer cal. |
Return Type |
Boolean |
Default |
False |
Examples |
phaseRef.IncludeUnknownMixer = True |
value = phaseRef.IncludeUnknownMixer 'Read |
|
C++ Syntax |
HRESULT get_IncludeUnknownMixer(VARIANT_BOOL *value) HRESULT put_IncludeUnknownMixer(VARIANT_BOOL value) |
Interface |
IPhaseReference2 |