Write/Read
About Interpolation

InterpolateMemory Property


Description

Sets and reads the state of the memory data interpolation. Learn more.

 VB Syntax

meas.InterpolateMemory = bool

Variable

(Type) - Description

meas

A Measurement (object)

bool

(boolean)
False
- Turn memory data interpolation OFF.

True - Turn memory data interpolation ON.

Return Type

Boolean

Default

False

Examples

meas.InterpolateMemory = True 'Write
state = meas.InterpolateMemory 'Read

C++ Syntax

HRESULT get_InterpolateMemory(VARIANT_BOOL *intState)
HRESULT put_InterpolateMemory(VARIANT_BOOL intState)

Interface

IMeasurement18