Write/Read
About Interpolation

Interpolate Correction Property


Description

Turns ON and OFF correction interpolation which calculates new error terms when stimulus values change after calibration.

When this property is ON and error correction is being applied, the calibration subsystem attempts to interpolate the error terms whenever the stimulus parameters are changed.

When this property is OFF under the same circumstances, error correction is turned OFF.

 VB Syntax

meas.InterpolateCorrection = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(boolean) - Choose from:

True - Turns correction interpolation ON

False - Turns correction interpolation OFF

Return Type

Boolean

Default

True

Examples

meas.InterpolateCorrection = False

calInterpolate = InterpolateCorrection 'Read

C++ Syntax

HRESULT get_InterpolateCorrection(boolean *pVal)
HRESULT put_InterpolateCorrection(boolean newVal)

Interface

IMeasurement