Read-only |
About Balanced Measurements |
Description |
Returns whether or not the specified logical port number is balanced. |
VB Syntax |
value = chan.IsBalanced(logicalPort) |
Variable |
(Type) - Description |
balTopology |
A BalancedTopology (object) |
value |
(boolean) - Returned value is either: False - Logical port number is NOT balanced. True - Logical port number IS balanced. |
logicalPort |
(Long Integer) Logical port number. |
Return Type |
Boolean |
Default |
Not Applicable |
Examples |
'In the following example, 6 logical ports are mapped to 8 physical VNA ports. |
C++ Syntax |
HRESULT get_IsBalanced(long logicalPort, VARIANT_BOOL *bBalanced); |
Interface |
IBalancedTopology3 |