Read-only
About Trigger

IsContinuous Property


Description

Returns whether or not a channel is in continuous mode. To set the channel to continuous mode, use Continuous Method.

 VB Syntax

value = chan.IsContinuous

Variable

(Type) - Description

value

(boolean) - Choose either:

False - Channel trigger is NOT set to continuous.

True  - Channel trigger IS set to continuous.

chan

Channel (object)

Return Type

Boolean

Default

Not Applicable

Examples

trig = chan.IsContinuous 'Read

C++ Syntax

HRESULT get_IsContinuous ( VARIANT_BOOL *bContinuous);

Interface

IChannel4