Read only
About VNA Options

IsFrequencyOffsetPresent Property


Description

Returns a value indicating the presence of Frequency Offset Option S93080A in the remote VNA.

 VB Syntax

value = cap.IsFrequencyOffsetPresent

Variable

(Type) - Description

value

(Boolean) - Variable to store the returned value

True - Frequency Offset Option S93080A is present

False - Frequency Offset Option S93080A is not present

cap

A Capabilities (object)

Return Type

Boolean

Default

Not Applicable

Examples

value = cap.isFrequencyOffsetPresent(1) 'Read

C++ Syntax

HRESULT get_IsFrequencyOffsetPresent(VARIANT_BOOL * present );

Interface

ICapabilities