| Read/Write | About Embedded LO | 
| Description | Sets and returns the ON |OFF state of Embedded LO. | 
| VB Syntax | obj.IsOn = value | 
| Variable | (Type) - Description | 
| obj | An EmbeddedLO (object) or A ConverterEmbeddedLO (object) | 
| value | (Boolean) False - Turns Embedded LO OFF True - Turns Embedded LO ON | 
| Return Type | (Boolean) | 
| Default | False (OFF) | 
| Examples | embedLO.IsOn = True 'write | 
| data= embedLO.IsOn 'read | |
| C++ Syntax | HRESULT get_IsOn( VARIANT_BOOL* IsOn); HRESULT put_IsOn( VARIANT_BOOL IsOn); | 
| Interface | IEmbededLO |