Read only
About VNA Options

IsReceiverStepAttenuatorPresent Property


Description

Returns a value indicating the presence of Receiver step attenuators in the remote VNA.

 VB Syntax

value = cap.IsReceiverStepAttenuatorPresent (n)

Variable

(Type) - Description

value

(Boolean) - Variable to store the returned value.

True - Receiver step attenuators are present.

False - Receiver step attenuators are not present.

cap

A Capabilities (object)

n

(Long) - port number to query for step attenuators

Return Type

Boolean

Default

Not Applicable

Examples

value = cap.IsReceiverStepAttenuatorPresent(1)'Read

C++ Syntax

HRESULT get_IsReceiverStepAttenuatorPresent(long portNumber, VARIANT_BOOL *  present );

Interface

ICapabilities