Write/Read |
About Time Domain |
Description |
Sets or returns the Kaiser Beta of Time Domain transform windows |
VB Syntax |
trans.KaiserBeta = value |
Variable |
(Type) - Description |
trans |
A Transform (object) |
value |
(single) - Kaiser Beta. Choose any number between 0 and 13. |
Return Type |
Single |
Default |
0 |
Examples |
trans.KaiserBeta = 6 'sets the Kaiser Beta of a transform window -Write |
KB = trans.KaiserBeta 'Read |
|
C++ Syntax |
HRESULT get_KaiserBeta(float *pVal) |
Interface |
ITransform |