Read/Write |
About Embedded LO |
Description |
Sets and returns LO Frequency Delta. There is usually no need to set this value. Read this value to determine the difference between the LO Frequency that is stated in the Mixer dialog box and the last measured LO Frequency. |
VB Syntax |
obj.LOFrequencyDelta = value |
Variable |
(Type) - Description |
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
value |
(Double) LO Frequency delta in Hertz. |
Return Type |
(Double) |
Default |
Not Applicable |
Examples |
embedLO.LOFrequencyDelta = 0 'write |
value = embedLO.LOFrequencyDelta 'read |
|
C++ Syntax |
HRESULT get_LOFrequencyDelta(double* val); HRESULT put_LOFrequencyDelta(double val); |
Interface |
IEmbededLO |