Write/Read |
About Modifying Cal Kits |
Description |
Sets and Returns the label for the calibration standard. The label is used to prompt the user to connect the specified standard. |
VB Syntax |
calstd.Label = value |
Variable |
(Type) - Description |
calstd |
A CalStandard (object). Use calKit.GetCalStandard to get a handle to the standard. |
value |
(string) - between 1 and 12 characters long. Cannot begin with a numeric. |
Return Type |
String |
Default |
Not Applicable |
Examples |
calstd.Label = "Short" 'Write |
stdLabel = calstd.Label 'Read |
|
C++ Syntax |
HRESULT get_Label(BSTR *pVal) |
Interface |
ICalStandard |