Write/Read
About PMAR

LimitFrequency Property


Description

Enable or disable the use of the power meter min and max frequencies.

 VB Syntax

pwrSensor.LimitFrequency = value

Variable

(Type) - Description

pwrSensor

A PowerSensorAsReceiver (Object) or

a PowerSensor (Object)

value

(Boolean) - State of min and max frequency use. Choose from:

False - Min and max frequencies disabled.

True - Min and max frequencies enabled.

Return Type

Boolean

Default

False

Examples

pwrSensor.LimitFrequency = False 'Write

limit = pwrSensor.LimitFrequency 'Read

C++ Syntax

HRESULT put_LimitFrequency(VARIANT_BOOL newVal);

HRESULT get_LimitFrequency(VARIANT_BOOL* pVal);

Interface

IPowerSensorAsReceiver

IPowerSensor