Read-only
About Limit Testing

LoadPort Property


Description

Returns the load port number associated with an S-parameter reflection measurement.  If the measurement is not a reflection S-parameter, the number returned by this property will have no meaning.

 VB Syntax

loadPort = meas.LoadPort

Variable

(Type) - Description

loadPort

(long integer) - The reflection measurement’s load port number.

meas

A Measurement (object)

Return Type

Long Integer

Default

Not Applicable

Examples

Set meas = pna.ActiveMeasurement
loadPort = meas.LoadPort

C++ Syntax

HRESULT get_LoadPort(long *pPortNumber);

Interface

IMeasurement