Write/Read |
About Power Limit |
Description |
Enables or disables the ability to change the power limit values through the user interface. |
VB Syntax |
gpl.Lock = state |
Variable |
(Type) - Description |
gpl |
A GlobalPowerLimit (object) |
state |
(boolean) False - Disables the ability to change the power limit values from the user interface. True - Enables the ability to change the power limit values from the user interface. |
Return Type |
Boolean |
Default |
False |
Examples |
gpl.Lock = True 'Write |
UILock = gpl.Lock 'Read |
|
C++ Syntax |
HRESULT get_Lock(BOOL *pVal) |
Interface |
IGlobalPowerLimit |