Write/Read |
About Modifying Cal Kits |
Description |
Sets and Returns the insertion loss for the calibration standard. |
VB Syntax |
calstd.loss = value |
Variable |
(Type) - Description |
calstd |
A CalStandard (object). Use calKit.GetCalStandard to get a handle to the standard. |
value |
(single) - Insertion loss in Gohms / sec. (Giga Ohms per second of electrical delay) |
Return Type |
Single |
Default |
Not Applicable |
Examples |
calstd.loss = 3.5 'Write 3.5 Gohms of loss |
stdLoss = calstd.loss 'Read the value of Loss |
|
C++ Syntax |
HRESULT get_Loss(float *pVal) |
Interface |
ICalStandard |