Write/Read |
About Limit Lines |
Description |
Set and return whether Coupled Markers is set to ON or OFF after Preset. Learn more about Coupled Markers. |
VB Syntax |
pref.MarkCoupPresetIsOn = value |
Variable |
(Type) - Description |
pref |
A Preferences (object) |
value |
(Boolean) - Choose from: True - Coupled Markers is ON after Preset. False - Coupled Markers is OFF after Preset. |
Return Type |
Boolean |
Default |
False |
Examples |
pref.MarkCoupPresetIsOn = True 'Write |
value = pref.MarkCoupPresetIsOn 'Read |
|
C++ Syntax |
HRESULT get_MarkCoupPresetIsOn (VARIANT_BOOL* preference); HRESULT put_MarkCoupPresetIsOn (VARIANT_BOOL val) |
Interface |
IPreferences15 |