Write/Read |
About Marker Readout |
Description |
For the X-axis (stimulus), sets the number digits to display after the decimal point in marker readouts. |
VB Syntax |
win.MarkerReadoutStimulusPlaces = value |
Variable |
(Type) - Description |
win |
A NAWindow (object) |
value |
(Long Integer) Number of digits to display. Choose a value between 2 and 6. |
Return Type |
Long Integer |
Default |
3 |
Examples |
win.MarkerReadoutStimulusPlaces = 2 'Write value = app.ActiveNAWindow.MarkerReadoutStimulusPlaces 'Read |
C++ Syntax |
HRESULT get_MarkerReadoutStimulusPlaces(long *pVal) HRESULT put_MarkerReadoutStimulusPlaces(long newVal) |
Interface |
INAWindow3 |