Write/Read
About Marker Readout

MarkerReadoutXPosition Property


Description

Sets the X-axis position of marker readouts. Readouts are right-justified at the specified position.

 VB Syntax

win.MarkerReadoutXPosition = value

Variable

(Type) - Description

win

A NAWindow (object)

value

(Double) X-axis position. Choose a value between 1 (far left) and 10 (far right).

Return Type

Double

Default

10

Examples

win.MarkerReadoutXPosition = 3 'Write

value = app.ActiveNAWindow.MarkerReadoutXPosition 'Read

C++ Syntax

HRESULT get_MarkerReadoutXPosition(double *pVal)

HRESULT put_MarkerReadoutXPosition(double newVal)

Interface

INAWindow3