Write/Read
About Marker Readout

MarkerSymbol Property


Description

Sets the symbol to display for marker position.

 VB Syntax

win.MarkerSymbol = value

Variable

(Type) - Description

win

A NAWindow (object)

value

(Enum as naMarkerSymbol) Choose from:

0 - naMarkerSymbolTriangle

1 - naMarkerSymbolFlag

2 - naMarkerSymbolLine

See pictures of symbols

Return Type

Enum

Default

0 - naMarkerSymbolTriangle

Examples

win.MarkerSymbol = naMarkerSymbolLine 'Write

value = app.ActiveNAWindow.MarkerSymbol 'Read

C++ Syntax

HRESULT get_MarkerSymbol(double *pVal)

HRESULT put_MarkerSymbol(double newVal)

Interface

INAWindow3