Write/Read
About Diff I/Q App

MatchFrequencyRange Property


Description

Sets and reads the existing frequency ranges over which Match Correction is to be performed.

On the Source Configuration dialog under Match Correction, this is the Match Frequency Range setting.

 VB Syntax

DIQ.MatchFrequencyRange (port) = value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

port

(String) Source port name. Use SourcePortNames to read a list of valid source ports.

value

(String)  Frequency ranges, including the "F<n>", where <n> is the range number. Separate each range with a comma.

Return Type

String

Default

Depends on <port>

Examples

oDIQ.MatchFrequencyRange("port 1") = "F1,F2,F3"

Value = oDIQ.MatchFrequencyRange("port 2") 'Read

C++ Syntax

HRESULT get_MatchFrequencyRange(BSTR port, BSTR* MatchFrequencyRange);

HRESULT put_MatchFrequencyRange(BSTR port, BSTR MatchFrequencyRange);

Interface

IDIQ