Write/Read |
About External DC Devices |
Description |
Sets and returns the "Define Max As" value for an external DC Source. |
VB Syntax |
extDC.MaxOutput = value |
Variable |
(Type) - Description |
extDC |
A ExternalDCDevice (object) |
value |
(Double) Maximum value for the external DC Source. |
Return Type |
Double |
Default |
10 V |
Examples |
extDC.MaxOutput = 10 'Write value = extDC.MaxOutput 'Read |
C++ Syntax |
HRESULT get_MaxOutput( double* value); HRESULT put_MaxOutput( double value); |
Interface |
IExternalDCDevice3 |