Read-only
About Pulsed Application

MaximumIFFrequency Property


Description

Returns the Maximum allowed value for the IFFrequency Property

 VB Syntax

value = IfConfig.MaximumIFFrequency

Variable

(Type) - Description

value

(double) Variable to store the returned maximum allowed frequency that can be applied to the IFFrequency Property.

IfConfig

IFConfiguration (object)

Return Type

Double

Default

Not Applicable

Examples

val = App.ActiveChannel.IFConfiguration.MaximumIFFrequency 'Read

C++ Syntax

HRESULT get_MaximumIFFrequency( double * pMaxFreq);

Interface

IIFConfiguration3