Read only
About VNA Options

MaximumNumberOfPoints Property


Description

Returns the maximum possible number of data points.

 VB Syntax

value = obj.MaximumNumberOfPoints

Variable

(Type) - Description

value

(Long) - Variable to store the returned maximum value for number of points.

cap

A Capabilities (object)

or

A GainCompression (object)

Return Type

Double

Default

Not Applicable

Examples

value = cap.MaximumNumberOfPoints 'Read

C++ Syntax

HRESULT get_MaximumNumberOfPoints(double *  maximumNumberOfPoints );

Interface

ICapabilities

IGainCompression