Read only
About VNA Options

MaximumReceiverStepAttenuator Property


Description

Returns the maximum amount of receiver attenuation.

 VB Syntax

value = cap.MaximumReceiverStepAttenuator (n)

Variable

(Type) - Description

value

(Double) - Variable to store the returned value of maximum receiver attenuation.

cap

A Capabilities (object)

n

(Long) - port number to query for step attenuators

Return Type

Double

Default

Not Applicable

Examples

value = cap.MaximumReceiverStepAttenuator'Read

C++ Syntax

HRESULT get_MaximumReceiverStepAttenuator(long portNumber, double *  attenuation );

Interface

ICapabilities